Tools


MobilityMobility

Contact
Close Contact layer

Siemens AG, Sector Infrastructure & Cities

Division Mobility and Logistics

Otto-Hahn-Ring 6
D-81739 M�nchen

Telephone: +49 (89) 636 00

contact.mobility@siemens.com

Division Rail Systems

Nonnendammallee 101
D-13629 Berlin

Telephone: +49 (30) 386 0

siemensrailsystemscontact.ic@siemens.com

Division Smart Grid Rail Electrification

Mozartstr. 33b
D-91052 Erlangen

Telephone: +49 (30) 386 0

electrification.mobility@siemens.com


References
Close References layer
Reference Database

Reference database

Explore our Reference Database that allows you to perform quick and detailed searches for references. You can select various search criteria and combine them together.

Visit our Database

Green mobility at the airport

Innovative logistics systems improve energy efficiency, while at the same time increasing productivity – for example, powerful conveyor systems that quickly and reliably transport baggage. At Incheon International Airport, the largest in South Korea, over 56,000 pieces of baggage are sorted and distributed every hour by baggage handling systems from Siemens operating with highly efficient geared motors with efficiency levels between 94 and 96 percent.

Baggage transport and sorting systems

The Sibag Cross baggage sorting system ensures fast and safe baggage handling in airports. The hybrid tray solution is a combination container system and crossbelt conveyor. The belt moves without an electric motor, which means reduced energy consumption and low operating costs – with a highly reliable and flexible system.

Airport management system

Siemens and the Deutsches Zentrum für Luft- und Raumfahrt (DLR – German Aerospace Center) worked together to develop Siamos, the Siemens Airport Management and Operations Software that flexibly adapts airport operation to managerial goals. Siamos permits direct energy savings and a sustained increase in efficiency. The Vienna International Airport, for example, was able to achieve energy savings of over 20 percent. Further advantages of Siamos include five tons less jet fuel consumed per hour and runway thanks to shorter waiting times. In addition, flights are up to 20 percent more punctual.

Fully automated passenger transport

The fully automated passenger transport systems from Siemens have the capacity to transport 30,000 passengers per hour and direction. Another advantage of the vehicles being used for Airval airport shuttles and Cityval trains is their low energy consumption. The vehicle brakes are operated electrically and the braking energy is stored for subsequent accelerations.

Links to airports

Rail connections to and from airports are a reliable and attractive alternative to traveling by private car or taxi. At the same time, they help reduce pollution in urban centers. And if, for example as in Bangkok, you can check your bags in the city, the system is especially convenient for passengers. Thanks to an innovative logistics system from Siemens, baggage is automatically loaded onto the Airport Rail Link, transported to the airport in an environmentally responsible manner, and then transferred to the baggage system.