Customer benefit

The City of Oslo is Convinced

After already 83 three-car metro trains were commissioned into operation on the rail network of 85 kilometers, the city of Oslo ordered in 2010 additional 32 trains.

  • 25 % less energy consumption in comparison to the predecessor model

  • An operating train which is fully occupied has a CO2 emission rate of only
     0.3g per passenger per km

  • The recycling rate of 94.7 % reduces the emission by an additional 405
    tons per train due to the saving in primary resources


Excellent conceptional framework: Amongst others, the Metro Oslo from Siemens was honored with the "Sustainable Product Award" of the Technical University in Vienna, the EEP Award, and the Createch Award.