Intelligent traffic management

Connect systems and data to optimize traffic flow
Intelligent traffic management allows you to ensure mobility both for today and for tomorrow, and it will enable you to efficiently manage growing traffic volumes and environmental impact.
With traffic management, cities can plan and act proactively
To keep or regain their appeal in a sustainable way, cities and regions have to address traffic and its impact on people and the environment. Strategies need to include not only switching to other modes of transportation, but also to intelligently manage road traffic. Experience has shown that simply reacting to impaired traffic routes after damage has occurred is not enough. Predictive planning is essential for optimally utilizing the capacity of the traffic network, and it should include situations such as a scheduled event that is associated or traffic limits due to pollution thresholds.
We support cities and municipalities in integrating and evolving intelligent strategies into their traffic systems so that traffic managers can proactively direct traffic with virtual signage, connecting infrastructure and vehicles, and other innovative solutions.
Redesign mobility
For a sustainable mobility, managing the capacities of roads and traffic routes has to be holistic, predictive and focused on actual demand. Traffic managers need to reconcile multiple aspects such as cost-effectiveness, convenience, safety, and environmental protection. The prerequisite for this are data acquired from intelligent infrastructure systems, for example, from autonomous and connected vehicles. The information gained from these data helps use roads and transportation routes to their optimum capacity and to create incentives for commuters that help improve traffic flows and mobility behavior – including solutions for safer and more convenient urban bicycle traffic. The result is an attractive city with excellent mobility options that is both green and livable.
On your path to autonomous driving
A sustainable mobility requires connected information from infrastructure, vehicles, and commuters. This is what our Mobility Operating System was built for: combine and control all parts of the mobility network to make your city’s traffic safe for all stakeholders, including autonomous vehicles.