Locomotives

Mobility through adaptability

Our future-ready locomotives allow you to operate economically while reducing environmental impact and conserving resources. Whether you are seeking flexibility or require powerful locomotives for the heaviest transport tasks, we offer you individualized solutions that can be precisely tailored to your requirement profiles.

Europe

Locomotives for your exact requirements

Vectron

 

Meet Europe’s current and future transportation needs with locomotives that are exactly tailored to your requirements. Vectron features a full range of modular locomotives, from pure AC and DC locomotives up to MS locomotives and the dual-powered locomotive Vectron Dual Mode. The vehicle concept makes no compromises when it comes to modularity and can be precisely customized.
 

 

Smartron

 

The range of performance features in the Smartron is precisely tailored to freight transport within Germany. You benefit from optimally adapted performance with attractive terms and conditions.

 

North America

Powerful locomotives for North America

Charger

The diesel-electric Charger was developed for fast regional and main-line service. It complies with the strict Tier 4 emissions standards and guarantees economical and ecofriendly operation.
 

ACS-64

Amtrak ordered 70 ACS-64 electric locomotives, which it is now using to offer more reliable and efficient service in the Northeast and Keystone corridors. And now SEPTA has also opted for 15 ACS-64 locomotives.

Both Charger and ACS-64 reach a maximum speed of 200 km/h.

Russia

Full power for Russia

The 2ES7 and 2ES10 double locomotives were developed for heavy freight traffic in Russia. The 2ES10 is designed for operation under 3 kV DC and the 2ES7 under 25 kV/50 Hz. Among other things, both locomotives ensure low energy consumption thanks to energy recuperation and excellent performance: A two-section locomotive in the new design can replace an old three-section locomotive, thereby substantially increasing productivity. Over 150 locomotives have already been delivered.

Asia and Australia

Highest performance in freight traffic

The E40AC freight locomotive is designed for use in Australia’s heavy freight transport. Thanks to its superior performance, it significantly reduces the number of locomotives required: Five of the old locomotives can be replaced by three E40AC locomotives. 100 E40ACs are being deployed by three customers.

Middle East

Reliability as the way to the future

Reliable and environmentally friendly ER24PC locomotives are the answer to the challenges of future-ready mobility in Iran. For passenger transport in Iran, 150 state-of-the-art ER24PC locomotives were delivered that reach speeds of up to 160 km/h.

On-board sustainability

Green technology on rails

Whether freight or passenger transport, whether mass transit or main-line traffic – rails are the most environmentally friendly mode of transport. With our locomotives, we take it one step further and combine environmental protection with extreme cost-effectiveness – state-of-the-art, highly efficient, electric, and ecofriendly locomotives that use green technologies to constantly set new standards in freight and passenger transport.

Vectron – a model of sustainability

Energy-efficient production, environmentally friendly materials, and up to 98 percent recyclability – that’s what makes the Vectron locomotive generation so extraordinary. For example: After recycling, a Vectron electric locomotive weighing a total of 85t is reduced to only 1,700kg – the equivalent of a mid-sized European car.
 

A worthy model of sustainability:

  • Energy-efficient operation thanks to the Vectron Eco Cruise driver assistance system 
  • Environmental compatibility throughout the entire lifecycle
  • Use of converters with ecofriendly water-cooling and transformer coolants made with biodegradable ester
  • Compliance with the strictest emission guidelines for pollutants, particulate matter, and noise Regenerative braking system
Siemens locomotives – sustainability on track

Download brochure

Many years of experience

140 years of Siemens locomotives – a success story

Siemens is at home on the rails. For over 140 years, we’ve been connecting people and regions via rails, and we’re constantly setting new trends in development with sustainable, smart rail transport. It all began back in 1879 with the first electric railway from Siemens.
Expertise in manufacturing

Tradition meets know-how: At our locomotive plant in Munich-Allach

For more than 180 years, locomotives have been manufactured for the world market in Munich – a total of more than 22,000 to be exact. Today, we manufacture the Vectron at our locomotive plant in Munich-Allach using state-of-the-art production technologies as well as highly flexible assembly methods.

A look back at the plant

The plant today

140 years of traction technology

Innovation in traction electronics - paving the way for more efficient rail transport

Since the first electric railway, we have driven rail traffic forward, time and time again. This also applies to the field of traction electronics – a sector that has developed rapidly since the 20th century. Our developments here have always stood for optimal traction performance with reliable, economical and efficient operation.

Contact

Get a head start on sustainability – with locomotives from Siemens

Choose maximum performance coupled with maximum efficiency on rails. Our experts will be happy to help.