LED Retrofit for Wait Indicators

Energy saving LED Wait Indicator retrofit solution
The Central Light Source (CLS) LED Wait Indicator retrofit solution enables existing Siemens and Peek 48-volt incandescent Wait indicators to be upgraded to the latest CLS LED technology. With its very low power consumption, the retrofit solution provides power savings typically in excess of 70% and represents a highly cost-effective upgrade option for existing Wait Indicators, particularly when undertaken alongside a wider LED traffic signal upgrade program.
In addition to easy installation, minimum waste and a full lamp monitoring compatibility with Siemens controllers, the new Central Light Source provides outstanding phantom performance with high optical brightness. It uses yellow LEDs, which offer improved visibility, particularly in bright sunlight.
The new CLS LED Wait indicators complement the existing Siemens retrofit solution for Helios and Peek Elite signals, allowing all signalling equipment on a site to be efficiently upgraded to modern LED technology, re-using as much of the existing roadside equipment as possible.
This enables customers to benefit from the overall energy savings of low power LED solutions and eliminates the ongoing need to regularly replace lamps, reducing the carbon footprint in both the lamp manufacturing process and the vehicle miles travelled to the site to undertake lamp changes.