Siemens Mobility Partners with L.K. Comstock to Digitalize NYC's Fulton-Liberty Lines with Advanced Signaling Technology

  • CBTC technology, Trainguard MT, boosting reliability to power faster, more frequent service 
  • Future-proofing one of NYC’s busiest subway corridors for decades of seamless operation
  • 25-year maintenance agreement for long-term reliability

Siemens Mobility’s CBTC technology will provide enhanced safety, on-time performance, capacity and scalability for trains running across the network. That means faster, more reliable service across New York.

Tobias Bauer, CEO of Siemens Mobility North America

Siemens Mobility, in collaboration with L.K. Comstock (LKC)—a premier electrical contractor specializing in rail transit systems—has been awarded a contract by the Metropolitan Transportation Authority (MTA) to modernize New York City’s Fulton-Liberty Lines with advanced Communications-Based Train Control (CBTC) technology.  

The Siemens CBTC System, Trainguard MT, in compliance with New York Subway Interoperability Interface Specifications (I2S) enables trains to run as close as 90 seconds apart, using next-generation signaling and continuous communication to keep operations moving seamlessly. This new technology is expected to boost capacity, reduce wait times, and provide the flexibility needed to meet future demand on these two busy subway lines, while preparing the network to keep New Yorkers on the move for decades to come. 

This transformative upgrade will connect 23 stations and replace nearly century-old infrastructure to enhance the commute across Brooklyn and Queens with an energy-efficient solution. Running primarily along a four‑track alignment, multiple trains can operate simultaneously on the Fulton-Liberty Lines—meaning that while together they span approximately 15 miles in length, the total track distance equates to nearly 40 track miles.  

“Modernizing the Fulton-Liberty Lines is more than a technology upgrade—it’s a step to improve the everyday commute for millions of New Yorkers,” said Tobias Bauer, CEO of Siemens Mobility North America. “Siemens Mobility’s CBTC technology will provide enhanced safety, on-time performance, capacity and scalability for trains running across the network. That means faster, more reliable service across New York.” 

“L.K. Comstock is proud to partner with Siemens Mobility and the MTA to deliver this critical upgrade to one of New York City’s most heavily traveled corridors,” said Ben D’Alessandro, President of L.K. Comstock. “Together, we are helping build a more resilient, higher-capacity transit system for the future.” 

 As part of the signal modernization, LKC will decommission all signaling and associated equipment that is replaced by the Train Control System. The scope of work includes the installation and replacement of 24 new Special Work Portions, 94 switch machines, and constructing four new train control rooms. These upgrades require four million feet of cable to be installed by LKC throughout the tunnels and within the newly built facilities.  

This project introduces 5G commuter cellular service, ensuring riders remain connected as they travel between stations. LKC will install a Distributed Antenna System and supporting fiber cabling in the underground tunnel portion of the project, which spans 62 track segments with work in 18 stations.    

Once the system modernization is complete, Siemens Mobility will also support its long-term performance and reliability through a 25-year maintenance commitment to the MTA with the option for two additional five-year extensions. This long-term partnership underscores a commitment to consistent, dependable service at the core of New York City’s transit future. 

The Fulton-Liberty Lines serve as vital arteries in New York City’s sprawling transit network. Starting at Jay Street-MetroTech Station, the Fulton Street Line travels through Central Brooklyn and then connects to the Liberty Avenue Line, which begins at Euclid Avenue Station and concludes in Ozone Park, Queens, linking multiple major subway lines along the way. Built in the 1930s and 1940s, this historic subway corridor is now at the heart of the MTA’s vision to create a future-ready and resilient transportation system. The A (Express) train runs along the Fulton-Liberty Lines for a significant portion of its route in Brooklyn and Queens, while the C (Local) train uses the Fulton Line for its entire route in Brooklyn. 

As part of the modernization project, Siemens Mobility will deploy Trainguard MT to seamlessly integrate nine subway interlockings across the two separate subway lines. This includes replacing outdated track circuits with innovative axle counter technology and introducing 5G-based radio communications to power real-time, optimized train control. 

With its North American headquarters located in New York City, Siemens Mobility and LKC have a deep-rooted relationship with the MTA and decades of experience delivering next-generation signaling and rolling stock technology to the region. This partnership not only strengthens the positions of Siemens Mobility and LKC as trusted advisors but also reinforces their commitment to shaping a more efficient and interconnected future for New York City’s transit system and the millions who rely on it every day. 

Contact for journalists 

Olivia Coffey  
Phone: (332) 213-7318; E-mail: olivia.coffey@siemens.com  

Amanda Fiorante 
Phone: (516) 269-1778, Email: afiorante@railworks.com  

For further information about Siemens Mobility in the U.S., please see: https://www.mobility.siemens.com/us/en.html  

Siemens Mobility is a separately managed company of Siemens AG. As a leader in intelligent transport solutions for more than 175 years, Siemens Mobility is constantly innovating its portfolio. Its core areas include rolling stock, rail automation and electrification, a comprehensive software portfolio, turnkey systems as well as related services. With digital products and solutions, and the use of industrial AI, Siemens Mobility is enabling mobility operators worldwide to make their infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience, and guarantee availability. In fiscal year 2025, which ended on September 30, 2025, Siemens Mobility posted revenue of €12.4 billion and employed around 43,400 people worldwide. Further information is available at: www.siemens.com/mobility 

RailWorks Corporation was founded in 1998, RailWorks Corporation provides track construction, electrical systems construction, and maintenance services throughout the United States and Canada for major transit authorities, Class I, short-line railroads, and rail-served commercial and industrial companies. Trusted RailWorks brands include L.K. Comstock, PNR RailWorks, and NARSTCO. For more information, visit www.railworks.com.