eHighway – Electrification of road freight transport

Road freight transport powered by electricity: Siemens’ dynamic charging infrastructure combines the efficiency of electrified railroads with the flexibility of trucks into an innovative freight traffic solution that is efficient, economical, and environmentally friendly.
Even under ambitious scenarios to shift goods transport to electrified rail, road freight is expected to grow in absolute terms and remain the biggest source of CO2 from freight. We all depend on trucks for goods and services we need in our daily lives. But 24% of global CO2 emissions are caused by transportation, and road freight transport plays a considerable role in these emissions. As we aim to cut emissions by 65% in Germany by 2030, and reach carbon neutrality in Europe by 2045, it is imperative to examine strategies that will contribute to significantly lower emissions in the transportation sector.
Siemens Mobility is conducting a comparison of technology concepts to reduce CO2 emissions in long-haul trucking, assessing the advantages and disadvantages in terms of economic and environmental impact by evaluating eight criteria: Operational Range, Time to Market, Scalability & Resource Efficiency, Energy Efficiency, Total Cost of Ownership, Flexibility, and CO2 Abatement Cost. Let’s take a look at the facts.
The logistics industry has an average daily mileage of 750 km, and today’s diesel trucks have a range of up to 2,300 km. Long-haul journeys above 500km almost exclusively are driven on highways. Interestingly, 89% of German trucks only drive 50 km or fewer when leaving the highway roads.
Our eHighway solution enables unlimited operational range within the infrastructure. Overhead contact line (OCL) trucks are equipped with a battery for additional electric range outside of the OCL infrastructure. In comparison, 40-ton Battery-electric trucks (BEV) have a maximum range of 200 km, Fuel-Cell Electric trucks (FCEV) have good potential for long-haul trucking, and trucks powered by Renewable Fuels (RF) have about the same range as conventional combustion engine trucks.
Reaching the ambitious CO2 emission goals for long-haul trucking requires a quick roll-out of proven technologies. Several alternative drives and fuel systems are in the works, but which technology can deliver the required impact in time?
The Siemens Mobility eHighway solution is based on mature technology and more than 100 years of overhead contact line (OCL) experience. The system has established supply chains and open standards. It can be implemented immediately to make a valuable contribution to reducing emissions in long-haul trucking.
To achieve the necessary CO2 reductions in time, it’s not enough for a technology to be available now: It also has to be possible to scale up quickly so that intermediate goals can be met: for example,70 percent of new semi-truck sales in 2030.
This challenge is one of “scalability,” and it depends on factors like the capabilities of the supply chains and the degree to which these capabilities can be quickly channeled into a rapid transformation of the road freight sector.
Closely related to the issue of scaling is the availability of natural resources. Especially during rapid growth in material demand, there’s a risk of supply bottlenecks that could hinder a timely, large-scale implementation.
It’s logical that the less energy needed, the better – for the economy and the environment. Decarbonizing road freight using alternative drive trains like fuel-cell electric vehicles (FCEVs) or using renewable fuels (RFs) come with significant inefficiencies in production, transportation, storage, and distribution.
Hybrid trucks and battery electric vehicles (BEVs) that are connected to overhead contact lines (OCLs) are the most energy-efficient, with well-to-wheel efficiency of around 73 percent. This offers distinct advantages over alternative fuels that are produced synthetically with renewable electricity
In the decarbonization of long-haul freight transport total cost of ownership (TCO) is a crucial criterion for businesses adopting new technologies. In road freight the TCO is heavily influenced by the cost of energy costs, but also the cost of the vehicle plays a major role. The cost of the new infrastructure is comparatively low, where the level of utilization is sufficiently high, as would be the case on busy corridors.
The Siemens eHighway solution has an expected utilization level similar to that of an existing highway. This, combined with the high energy efficiency and associated low cost of energy, yields strong operational savings. As trucks using the overhead contact lines (OCL) need less batteries, their acquisition cost is also comparatively low. High savings and low costs, makes it the most economical solution on the busy routes where most of the freight transport takes place.
Road freight forwarders face growing demands in areas like fuel costs, technology implementation, and sustainability. Shifting road freight to transport modes with lower carbon emissions is a complex undertaking that requires enormous flexibility in both approach and solution.
Overhead contact line (OCL) infrastructure is an upgrade of existing highways and provides truckers with a high degree of flexibility and security, including power supply for non-electrified routes. Adapting to OCL can take place one step at a time to meet growing demand and accommodate fleet management issues.
To meet the emission goals in the transportation sector, the most energy efficient and resource efficient solution needs to be implemented. Only a holistic approach will be able to accelerate a successful transition away from carbon-based transport, and that includes the full abatement cost of CO2.
Electrification is a proven, scalable option with lower abatement costs that takes advantage of existing infrastructures and technologies. Overhead contact lines (OCL) have been found to offer the lowest CO2 abatement cost for 40-ton tractor trucks in 2030. It also helps other alternative drive technologies overcome their main obstacles for wider adoption by offering dynamic charging.
Download our climate friendly road freight factsheet
Do you want to know more about the best strategy to achieve climate friendly road freight transportation?
In this report we present an objective analyse and give a comprehensive deep dive on the topic trough seven articles.
Let’s have a look at the facts!
Reduce truck operating costs and emissions
Implementing the dynamic charging infrastructure on the core highways creates a backbone solution for energy efficient, low cost, zero emission trucking that is complementary with other drive trains, fuels and transportation technology trends (e.g. automated or high-capacity vehicles). The eHighway system is applicable for various use cases.Shuttle transport
Heavily-used truck routes, for example from ports to freight and distribution centers, are often a burden on the environment. In these situations, the dynamic charging system produces a significant reduction in pollutant and CO2 emissions. At the same time, the economic benefits of the system are felt particularly quickly on these high-use routes.
- Solution for high frequency shuttle transport over short and medium distances (< 50 km), i.e. in ports or industrial areas
- Lower fuel consumption and longer lifetime
- Reduction of air and noise pollution
Electrified freight transport in mines
The eHighway is an ideal way to connect pits and mines with warehouses, transshipment points or processing plants. The economic benefits of the eHighway system can be easily calculated on the basis of transport volumes. At the same time, the eHighway system significantly reduces environmental pollution and dependence on fossil fuels.
- Connection of pits and mines to storage or transit locations
- Minimization of harmful emissions
- Sustainable, clean and economical mine operation
Electrified long-haul traffic
The dynamic charging system is based on a safe and proven infrastructure to provide a continuous energy supply to heavy commercial vehicles. It can be integrated and operated within the existing road infrastructure without significant effort and combines the efficiency of electrified railroads with the flexibility of trucks, halving energy consumption while maintaining full mobility. The system enables trucks to use renewable energy and can contribute significantly to reducing CO2 emissions. Both the ecological and economic advantages of the eHighway system grow with increased use of the route.
- Economical and sustainable alternative for road freight transport
- Significant reduction of CO2 emissions
- Substantial cost savings for freight carriers
How it works?
Benefits and highlights:
- Decarbonizing road freight transport
- Reduces local air pollution
- High energy efficiency lowers operating costs
- Rapid integration into existing infrastructure
- Proven technology ensures rapid employment
- Compatible with other drive technologies
- Trucks can operate completely electrically and at the same time charge their batteries while driving
- Can be scaled up quickly based on established supply chains