Digital S-Bahn Hamburg
Hamburg is growing! According to a recent forecast by the Hamburg Statistics Office, Hamburg will be home to more than 2 million inhabitants in 2031. S-Bahn Hamburg wants to offer all Hamburg residents, tourists and guests a quality mobility service. In view of the city's growth, but also the future above-average growth of up to 50% for the S-Bahn Hamburg due to the expansion of the S-Bahn network with additional lines, the core network of the S-Bahn Hamburg is reaching capacity limits.
If you wish to link to and/or quote from the text, please cite the following source: "eurailpress.de/eik".