Integration into a system project with multiple interface partners
The experience from the SCI-CC interface system integration project, which is intended as the future unified command and control interface at Deutsche Bahn, is shared. As such, the general conditions that apply to the system architecture and task sharing are discussed.
If you wish to link to and/or quote from the text, please cite the following source: "eurailpress.de/sd".