Risk analyses for obstacle detection in automatic driving

This article focuses on the risk analysis for the “preventing collisions with objects or people in automated systems” function block. After a short summary of the ATO-RISK project’s basic approach, this function block’s functional structure is first explained and the special risk analysis features according to the DIN VDE V 0831-103 methodology are then elaborated. Finally, an overview of the risk analysis results is presented and discussed.

Download Technical Article

If you wish to link to and/or quote from the text, please cite the following source: "eurailpress.de/sd".