Our booking system for MaaS: The Sales Platform
In order to offer travelers a sustainable mobility alternative to private cars, different means of transport need to be integrated into a MaaS system. The Sales Platform plays an important role here. Based on the Sales Platform, passengers can book and pay for tickets from different transport providers in one app.

In order to offer travelers a sustainable mobility alternative to private cars, different means of transport need to be integrated into a MaaS system. The Sales Platform plays an important role here. Based on the Sales Platform, passengers can book and pay for tickets from different transport providers in one app.
Interaction of MaaS components
Plan, book and ride.
Once intermodal travel planning is complete, the Sales Platform enables integrated booking and payment of tickets and mobility services. With the help of the app, travelers have access to all functions and always stay informed. All components are linked through interfaces and therefore work together smoothly.
Objectives of the Sales Platform
For the successful development of MaaS systems, all participants have to work together. This is only possible if everyone is also involved in the success of the platform.