Siemens Night Trains: Throughout Europe in the Sleeping Car

In order to achieve the agreed climate targets, the EU has agreed on a significant increase in sustainable transport. One option in long-distance rail transport for travel times of more than six hours is the night train. With this type of travel, a passenger train with special sleeping, couchette and/or seat cars is boarded at the starting point in the evening and, while the passengers sleep, covers a journey of up to 1400 km.

If you wish to link to and/or quote from the text, please cite the following source: "eurailpress.de/ei". 

Download article

Only available in German